Other Parts Discussed in Thread: DLP4710EVM-LC
Hi, how can I install batch file into non-volatile memory?
I want to use the DMD without connecting LED, but by default, the firmware expects there to be LEDs connected, so module will not power on correctly if it detects that these LEDs are not present.
When the LED is connected, I can turn on the DLP then click 'advanced' button on the GUI and add batch files. But when I disconnected the LED, then turn on the DLP and try to write batch file to tell the DLP that I want to use DMD without LED( W 36 52 00), it doesn't work.
So I need to change the batch file before I turn the DMD on, but how can I do that?
looking forward to your response, thanks so much