This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Higher level languages running on Angstrom

 

 

Is there a Basic compiler that runs on the Angstrom platform and can be used to control the Pico 2?  

Is there is a C++ compiler or any other languages that run on the Angstrom platform and can be used to control the Pico 2?

 

 

  • Alan,

    Yes. Any language which can be run on Linux can be run on the Angstrom distribution (and that means just about any computer language ever developed). We are not able to support questions about Angstrom or compiler questions. Your best resources would be the BeagleBoard and Angstrom support forums (http://groups.google.com/group/beagleboard and http://www.angstrom-distribution.org/).

    Best regards,

    Pascal