Other Parts Discussed in Thread: DLP2010, DLP500YX
Excuse me, I got these two boards a few days ago, but I want to ask about the connection method of the two boards. I tried to use the cable connection as shown in the picture, but the status of the GUI of my computer is shown as the picture. It seems that the DMD is not connected to the DLP board
DLP2010 tilt angle +17~-17
degree
DLP500YX tilt angle +17.5~-17.5 degree
What are the benefits of a larger tilt Angle range?