Modified device parameter file could handle the components. However it's not perfect, few of them would not work. Need to make sure proper value from Spec.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Modified device parameter file could handle the components. However it's not perfect, few of them would not work. Need to make sure proper value from Spec.
Hi Takeshi,
We need additional details to provide support on this.
1. Please share the modified device parameter file you are using.
2. When you say "it's not perfect, few of them would not work", what is the problem faced.
3. Yes. FlashDeviceParameters.txt file should match with the flash chip spec for proper operation.
Thanks,
Shivakumar
They added “M29W128G” in attached file.
The problem was they could not upload image into flash.
Hi Honzawa-san,
I think the attachment is missing.
Can you please attach the FlashDeviceParameters.txt file used.
Thanks,
Shivakumar
Hello Honzawa-san,
Do you have an update from your side on this request?
Thanks,
Matt
Thank for your support and sorry for late response.
Our customer said that they could not replicate the issue now.
I'll wait their response for a while.