Other Parts Discussed in Thread: DLP4500, DLPC350
I am trying to figure out what is the maximum number of 1bit images that I can upload to the flash memory of the DLP4500 EVM.
I have managed to replace one of the images with a bmp that I created using 24 1-bit images (the size of the bmp ends up being about 3 MB while each 1-bit image is about 1Mbit). However, I don't want to add more that the original 3 flash images because I am afraid I might brick the DLP4500.
I've read in the documentation (DLPC350 DLP® Digital Controller for DLP4500 and DLP4500NIR DMDs datasheet (Rev. F) - https://www.ti.com/lit/ds/symlink/dlpc350.pdf -) that the internal RAM memory is 64 Mbit (Stores up to 48 1bit images), and that it supports 32 MB of external parallel flash for increased pattern storage.
So to my questions:
Question 1:
The statement about the 32MB is a bit ambiguous to me. Is there 32MB of parallel flash on the DLP4500EVM?
Question 2:
If there are 32MB available would that mean that it is possible to upload about 10 24bit images (since one 24bit image is about 3MB)?
Thank you in advance.