This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DMD Discovery 1100

Other Parts Discussed in Thread: DLP7000, DLPC410, DLPC900

Dear Sirs,

I have two EVM board: Discovery 1100, very old DMD model.

But I have not TI software GUI & below doc to work with DMD 1100.

==========
Discovery 1100 Controller Circuit Card Assembly, Reference Design, TI DN 2506022
Discovery 1100 Controller Board GUI User’s & Programmer’s Guide, TI DN 2506021
Schematics - Discovery 1100, TI DN 2506026
Mechanical Drawings – DMD, Controller Board, mounting diagrams
Quick Start Guide, TI DN 2506025
===========

Could you please provide a link to the software & DOC?

Thank you in advance.

Best regards,

  • Hello Lee,

    Welcome to DLP forum and thank you for your interest in DLP Technology.

    The Discovery 1100 EVM has been end of life for more than a decade. There is no technical support for it. We don't have the firmware and documentation on it.

    We don't not recommend any development on discontinued product. Please use EVM from  current portfolio. If you could share your application requirements, I could suggest you appropriate DLP product.

    regards,

    Vivek

  • Hello Vivek.

    Thanks for reply.

    Currently, DMD UV-EVM is so expensive to buy.
    I'm just going to test the optical system using the usb port with Discovery 1100 EVM  that I have.


    Could you please provide a link to only the software? (the Window GUI Program of Discovery 1100 EVM)

    Thanks.

    regards,

    Hslee

  • Hello Lee,

    As Vivek mentioned, we no longer have the firmware or GUI or documentation for this platform which was written in the Windows 98/XP era.  

    Fizix

  • Mr. lee

    If you need the 405 nm optical performance and speed that the D1100 DMD DiscoveryTm 1100 product offered you can purchase up-to-date EVMs on TI.com

    DLP7000 DMD - DLPLCR70EVM

    DLPC410 Controller - DLPLCRC410EVM

    Or you can work with a lower cost higher resolution DMD family

    DLP6500 DMD - DLPLCR65EVM

    DLPC900 Controller - DLPLCRC900EVM