This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710EVM-LC: DLP4710-LC

Part Number: DLP4710EVM-LC


Hi,

We have Idenfied DLP4710-LC for our requirement

i have went through design files of DLP4710EVM-LC, also procured two nos of kits for evalaution

I wish to know following things

1. The BOM doensnt contain data of LEDs (R,G,B) used with the DLP Kit, Kindly let me know the MPN of it

2. For my application i wish to use three green leds, that means green leds in place of R and B, this will help me increasing the light output intensity for streaming a green image

3. Kindly let me know how to flash the TI image of DLPC if i make my own board from the schematics of DLP4710EVM-LC

  • Hello User,

    1.) The EVM is using the OSRAM P1W red, blue, and green LEDs.

    2.) Is there a specific concern here or a question you need answered?

    3.) There are two options available. You can either use the Light Control GUI after full assembly of the system or you can program the flash memory before it is placed on the board.

    I will send a friend request and I can message you in private over details.

    Regards,

    John