Other Parts Discussed in Thread: DLP4710EVM-LC, DLPC3479
Hi,
We have Idenfied DLP4710-LC for our requirement
i have went through design files of DLP4710EVM-LC, also procured two nos of kits for evalaution
My video input resolution is 1080p30 for which a DVI Rx is sufficient i may not require a HDMI Rx.
I wish to know following things
1. Can we replace the HDMI reciever IC with any TI IC(DVI Rx) ? is anything available ?
2. I wish to use the same binaries used for the DLP4710EVM-LC and replace the HDMI reciever IC with a DVI Rx IC
3. if above 1&2 are not possible and i am abided to buy on IT6801 kindly provide contact details of company