Other Parts Discussed in Thread: DLP6500FYE
Hello!
I have a DLPC900 with USB communication and I use it in pattern on the fly mode.
When I use the command 0x1A32 (as in 2.4.4.3.4, page 71 of the programmer's manual rev G) to reorder the Pattern LUT I get the following error: "Invalid command number : 0x1A32"
Here are the software revisions as read from the controller:
Application software revision: 2.0.0
API software revision: 4.1.101
Software configuration revision: 68.33.0
Sequencer configuration revision: 68.33.256
Hardware Configuration and Firmware Tag: DLPR900PROM-6500-v2.0.0ault
Is my firmware too old for this command?
Moreover, in table A-2 at page 90 of revision G of the programmers manual, "Pattern LUT Reorder Configuration" and "Pattern LUT Definition" are both listed with the same USB command: 0x1A34.
Thank you so much,
Marco