Hi,
My customer is currently designing a Terahertz modulation system. This requires a high end pixel modulator part such as DMDs. Resolution of approximately 1920x1080, and it must work in the 400-800nm range. Any specific region in that range is fine though more preferably around 532 or 800. In terms of operating it’s required that the DMD is capable of withstanding over 2W/cm^2 from said wavelength laser.
Does this DLP9500 application, or is there better that you can recommend?
Thank you.
Regards,
May