Hi,
I have been using LightCrafter (the one with DLP3000) for years as it works quite well in the 1-bit monochrome mode at 1140Hz.
Currently I want to get a new EVM that can update at a similar update rate (ideally more than 1000Hz) but with colours (e.g. 1-bit for each of RGB).
In terms of the native resolution, it would be great if it's 1080p or more but the lower resolution could be also fine because the update rate is the most important factor for me.
Could you please recomend which EVM is the most suitable for my case?
I have been looking for in your website but could not find information regarding the update rate in the user guides.
Additional info:
- It would be great if I can get some synchronization in/out pins for hardware-level synch.
- I would prefer to update the image through HDMI to make interactive applications.
Best regards,
Ryuji