This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710EVM-LC: DLP4710EVM-LC - Max pattern rate

Part Number: DLP4710EVM-LC
Other Parts Discussed in Thread: DLP3010EVM-LC

I have an application whereby I need to generate high-speed/high-resolution patterns in order to test a computer vision system. I have been looking at the DLP4710EVM-LC which I understand can project at 1080p resolution which is great. However, it is not clear to me what the maximum pattern generation rate would be for a binary pattern? Can you clarify this please? Is there a better model I should be looking at?

Thanks