Good morning,
I am looking for the maximum allowed input power supply: datasheet of the DLP provide only the following informations (see figure)
I want to know which voltage will be accepted by the DLP before it will be broken/damaged (the working range of the DPL: 12 V DC is not enough for me because I am going to design a DC protection and I need to know the maximum input voltage accepted by the device to best fit the protection).
Thank you for the support
Best Regards
Luigi Spurio