Part Number: DLPC3479
What are the timing constraints required for TRIG_IN?
The figure below is taken from the DLPC3479 datasheet, with T1 and T2 added.
In the figure, it is not clear at what timing Trigger In (TRIG_IN) should be input to display Pat1 and after.
・Are there any timing constraints on T1? (For example T1 > Tdarkpost)
・Is T2 always equal to Tdarkpre?