Dear Sir,
I'm using the DLP4710EVM-LC and once it power up, it default Tirgger mode (by Trigger IN) and display the internal pattern. I can use GUI to switch to the "external video source" so it can accept the HDMI signal (1920x1080 and 60Hz). But how can I set it default HDMI detection so I dont' need to connect to GUI every time when I power up the EVM ?
Thanks!
Vincent