Hi,
I'm testing DLP3010EVM-LC with custom optical engine.
It works well when I tested it using the display menu.
However, while testing the internal patterns mode, I got the following error message, saying:
Error EVM DMD Device ID does not match GUI Product ID
The EVM with the custom optical engine works fine when tested with the display menu.
What can be the cause of the problem and how can I test the the pattern with the EVM?
Thanks