Part Number: DLPDLCR230NPEVM
Other Parts Discussed in Thread: DLPC3436, DLPA2005
Hello,
I'm relatively new to this technology and am having trouble using the DLPDLCR230NPEVM.
I am using a raspberry pi 4b with the DLPDLCR230NPEVM. I am able to run all the scripts provided by TI in the python support, however no images appear when running. The only projection displayed is the initial "DLP Texas Instruments" logo on start up. I see the TI DLP logo, but no test pattern after it, like described in the manual. When I run the test patterns in "sample01_tpg.py", I can visibly see the DLP's mirrors change between the completely black and all-white projections, but no light is actually projected. On startup D_INIT_B and D_HOST_IRQ are always on, and D-DONE cycles with the projection of the DLP logo.
My Setup and things I've tried:
- I have installed gpio wiring and I can detect the DLPDLCR230NPEVM over i2c
- I re imaged the DLPDLCR230NPEVM using "flash_write_fpga.py" with dlpc3436_controller_firmware_7.3.13.img and "flash_write_controller.py" with dlpc3436_fpga_firmware_1.1.bin.
- I changed the gpio drive strength from (e.g. using "gpio drive 0 6") between 5,6,7
- I've changed power supplies from a wall plug 5V 3A to a 12V,30A PS with a 5V stepdown using a BUC converter
I'm a little confused and would appreciate some help. I've attached two images showing the startup behavior between the dlp logo and absence of the test pattern:
Thanks in advance!




When the DLP is powered, RESETz does start low and then rises, as seen in the attached photo: