Other Parts Discussed in Thread: DLPLCR4500EVM, , DLP4710LC, DLPC3479
Hi Team,
Our customer is looking for a DMD to do some patterned light generation. They want a DMD that can be controlled in a laboratory setting to generate patterned images by reflecting laser light off the DMD. A minimum rep rate of 20Hz is preferred with a chip size of at least .5”x.5” with 1000x1000 mirrors. Ideally they want a system that can be controlled using Python/Matlab.
It seems that the DLPLCR4500EVM is suitable their application, however, it is currently out of stocks. Can they use DLP4710EVM-LC instead? Does it support Python/Matlab?
Regards,
Danilo