Hello E2E Experts,
Good day.
I have a DLP6500FLQ .65” 1080p Type-A DMD, 400nm - 700nm that I am looking to establish LabVIEW control of. I was planning on using a DLL wrapper for the API commands from the 'DLP® Advanced Light Control Software Development Kit for LightcrafterTM Evaluation Modules User’s Guide.
However, the SDK listed on the DLP6500FLQ seems to be from 2016 and a bunch of the supporting software is 32-bit.
Is there a more up-to-date version of this SDK that is available or should I proceed with the one on the webpage for the DLP6500FLQ?
The system that this will run on is Windows 10 64-bit.
Thank you in advance for your support.
Regards,
CSC