Other Parts Discussed in Thread: DLPC3433
H Experts,
Asking your assistance on this case:
Customer would like to return the board which purchased two weeks ago. Reported that the DLPDLCR3010EVM board has an issue and there was a loud noise when they turned on.
The noise is related to the fan of the projector. They use 12V DV supply (max 3A). Another issue they reported with HDMI connection: Connected PC to the projector with HDMI cable to use this projector as a monitor, but do not see any image from the projector except Texas Instrument logo.
For your assistance.
Thank you.