Other Parts Discussed in Thread: DLP9000
The DLPLCR900EVM does not boot up properly when connected to power.
The D8 '+12V GOOD' and D9 'POWERGOOD' LEDs are supposed to turn green when connected to power but only the D8 one does. Following this the D6 LED is supposed to be toggling on and off indicating the DLPC900 controller successfully booted up but it doesn't, indicating there is problems with booting up.
I have connected the evaluation module to a +12V power supply as indicated.
Please let me know if you can help.
Many thanks,
Valentina