This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010EVM-LC: How to add 1bit pattern set as start up to firmware

Part Number: DLP3010EVM-LC

Hello,

I have a pattern set that contains 26 1-bit patterns. I want to combine this with existing firmware so that the device can auto display the pattern set as long as it is powered. I do have some struggles on the Edit firmware. For the step3 Splash image, should I put my pattern set in here or I should put it in the advanced settings. I left the step 3 as blank and fill the advanced with my pattern data file generated from internal pattern. The problem is that with this new firmware, the device does not play the pattern set automatically. Can you tell me the detailed and correct steps on this?

Thank you very much!

Yuchen