Hi~
What is the Memory size for DLPC230-Q1 on-chip SRAM?
How many frames in 1 Second for the DLPC230-Q1 Video Input Interface?
Many thanks & Best Wishes
Weite
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi~
What is the Memory size for DLPC230-Q1 on-chip SRAM?
How many frames in 1 Second for the DLPC230-Q1 Video Input Interface?
Many thanks & Best Wishes
Weite
The DLPC230 SRAM is designed to manage the maximum DMD size of 1152x1152. (0.55" DMD) and support a frame rate of 60Hz.
See the datasheet section 6.15 for more details. https://www.ti.com/lit/ds/symlink/dlpc230-q1.pdf
Does this answer your question?
Thanks,
Jason
Hello Weite -
This chipset has a one frame latency: so 16.67ms for a 60Hz video frame.
Regards,
Ross