Other Parts Discussed in Thread: DLPA3005, DLPC3439, DLPDLCR4710EVM-G2
Hi,
I have a DLP4710-G2 with controller DLPC3439 and driver DLPA3005.
I want to write an auto-init routine in which the RGB channels are turned OFF.
And this should be the command in the Batch file.
# Write: WRITE LED ENABLE = 7. DISABLE = 0
W 36 52 00
The batch file works if I run it in the advanced mode of the LightCrafter software, but if I try to update the image with the auto-init batch file, the batch file does not seem to run.
I followed the procedure described here:
https://e2e.ti.com/support/dlp-products-group/dlp/f/dlp-products-forum/749879/dlp3010evm-lc-dlp3010evm-lc-configure-auto-init-routine
Can you give me a suggestion in order to do that?
Thank you
Donato