We are trying to use the internal streaming mode, but it seems that we have to connect the DLP to a computer and send the command via I2C port to run it. Is it possible to run the internal patterns automatically after we powered up the DLP and do not connect to a processor?
I tried to use the batch files, but it confused me because it seems that there are still I2C commands in batch files. So does it means we have still to connect the DLP to a processor to run the batch files?