This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710LC:Custom build DLP chipset with DLP 4710LC

Part Number: DLP4710LC
Other Parts Discussed in Thread: TIDA-080005

Hello all,

We want to use DLP 4710LC in our laser system for realizing structured light.

But, we are able to find only DMD (DLP4710LC) and controller (DLPC 3479) for the parts needed to use DLP 4710LC component.

We have light source so just want to use custom build chipset excluding light sources in a commercially available DMD system (DLP4710LC-EVM).

Additionally, we want to connect the DMD system and computer to controll the light pattern

For this purpose, what additional components do we need?

If the custom build system using DLP4710LC is not available, could you tell me the components of custom build system using DLP 4710?

Best Regards,

HeeJu Son