HI, I'm trying to boot up to a new DLPC6540 projector using the following workflow:
- Connect to power via 24V PSU
- Connect to my laptop via a USB to TTL connector (this one)
- Use pySerial to send serial commands over TTL.
- Use ser.write([0x2a,0xfa,0x0d]) to power on the projector
I get no response that the projector has turned on though. I don't get a response via TTL and no fans/LEDs turn on in the projector. I also don't see where this information is located in the TI Programmer's Guide.
I am using this documentation from a Chinese manufacturer.