The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010EVM-LC:Regarding the change of the DLP's transient current limit.

Part Number: DLP3010EVM-LC
Other Parts Discussed in Thread: DLPA2005, DLPC3478

Hello, I'm yongjin.

I am working on a project by configuring DLPC3478, DLPA2005 and DMD3010.

I want to fix the problem that when the DLP RGB LED turns on, the current rises momentarily and then stabilizes.

Looking at the datasheet, there is a transient current limiting function, but I don't know how to use it.

In the meantime, I checked the forum and confirmed that TI directly modified and sent the FW.

I also want to receive the modified FW. I want to set the transient current limit of the RGB LED to 2550mA.

Reply please. thank you.