Part Number: DLPDLCR2000EVM
Other Parts Discussed in Thread: DLPDLCR230NPEVM
Hi,
We bought several DLCDLCR2000EVM interfaced using a custom PCB to a raspberry pi W. There was no issue.( mid 2020)
The issue we are seeing are in the newly order DLP module. We are thinking it might be related to the different firmware on the device : https://software-dl.ti.com/dlp/pico-fw-selector/release_notes/FWSel_DLPC2607_DLPA1000_pm1_i2c0x36_v1p2p6.html
Here is the setup :
DLPDLCR2000 EVM -> custom PCB -> Raspberry PI W (Raspbian GNU/Linux 10 (buster) Lite CLI only)
Config.txt :
# Added to support DLP2000 hdmi_force_hotplug=1 dtoverlay=i2c-gpio,i2c_gpio_sda=23,i2c_gpio_scl=24,i2c_gpio_delay_us=2 dtoverlay=dpi18 overscan_left=0 overscan_right=0 overscan_top=0 overscan_bottom=0 framebuffer_width=640 framebuffer_height=360 enable_dpi_lcd=1 display_default_lcd=1 dpi_group=2 dpi_mode=87 dpi_output_format=458775 hdmi_timings=640 0 50 35 10 360 0 30 35 10 0 0 0 60 0 19200000 3
i2C command for initialization. Note that we are running without the LED attached to the EVM explaining the multiple register write :
raspi-gpio set 22 op raspi-gpio set 22 dl sleep 0.1 raspi-gpio set 22 dh sleep 0.5 #Set 3 LEDs to 0 on DLP2607, start comm with DLPA1000 and propagate i2cset -y 11 0x1b 0x12 0x00 0x00 0x00 0x00 i i2cset -y 11 0x1b 0x13 0x00 0x00 0x00 0x00 i i2cset -y 11 0x1b 0x14 0x00 0x00 0x00 0x00 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x00 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD3 i #Turn off current directly on PAD1000 i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x03 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD0 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x00 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD2 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x04 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD0 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x00 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD2 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x05 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD0 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x00 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD2 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x06 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD0 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x00 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD2 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x07 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD0 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x00 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD2 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x08 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD0 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x00 i #Mask all off i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x0D i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD0 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0xDF i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD2 i sleep 0.1 #Turn on DLPA i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD0 i i2cset -y 11 0x1b 0x39 0x00 0x00 0x00 0x03 i i2cset -y 11 0x1b 0x3A 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x38 0x00 0x00 0x00 0xD2 i sleep 0.1 #UNPARK DMD i2cset -y 11 0x1b 0x2d 0x00 0x00 0x00 0x00 i #setup i2cset -y 11 0x1b 0x0b 0x00 0x00 0x00 0x00 i i2cset -y 11 0x1b 0x0c 0x00 0x00 0x00 0x1b i i2cset -y 11 0x1b 0x1E 0x00 0x00 0x00 0x01 i i2cset -y 11 0x1b 0x0d 0x00 0x00 0x00 0x02 i
Here is the issue we are having. every VSYNC, there is a blink in the image. We are sending full 640x360 white pixel. We are also sending full 640x360 black Pixel. All data line have been probed direclty on DLPDLCR2000EVM and are exactly the same. Using a constant LED illumination on the DMD. you can see the photodetector glitching every VSYNC :
WHITE IMAGE, image turns black on VSYNC : Note that this is not visible with bare eye as the pulse is very short.


BLACK IMAGE, image turns white on VSYNC :

Again, we are not seeing this issue with our old board (more then 1 board tried).
There is now way we can find the older firmware (1.2.5) Online.
If you can identify another source for this issue, we would be happy to try. We have swapped multiple element, cable, DMD, Only the new DLPDLCR200 boards are displaying the issue.
Thanks,
Christophe