This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3021-Q1: Does the firmware of the FPGA have basic temperature protection mechanisms?

Part Number: DLP3021-Q1

Dear team,

Does the firmware of the FPGA have a basic temperature protection mechanism?

Or does the FPGA simply store temperature in a temporary register?

Thank you for your assistance.

  • Hi Johns,

    The DLP3021-Q1 FPGA firmware only has the ability to read the temperature, but does not have any built-in response mechanism for over/under temperature protection. It is up to the external system controller to take responsive/corrective system action (e.g. disable LEDs or decrease LED PWM duty cycle) based on the temperature data captured by the FPGA.