This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR230NPEVM: Achieving 960x540 240hz with dlpdldcr230npevm

Genius 12000 points
Part Number: DLPDLCR230NPEVM


Dear team,

 I've attempted to follow the forum posts regarding achieving 240hz, to no avail.

config.txt: <attached>
init_parallel_mode.py: <attached>
Raspberry Pi 4b
I've attached my config.txt (modified 240hz timings recommended from here:)
Also attached the modified init_parallel_mode.py (from the same post)

My display is working (for desktop) at correct resolution (output from tvservice -s: state 0x400000 [LCD], 960x540 @ 60.00Hz, progressive), but the incorrect hz.
All test scripts function as expected.
Best Regards,
William