This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC7540EVM: Device cannot be detected anymore

Part Number: DLPC7540EVM
Other Parts Discussed in Thread: DLP650TE, DLPC7540

Hi! 

Recently we started working with DLPC7540EVM controller board and DLP650TE DMD. Following the DLP Display DLPC7540 4K  UHD EVM User's Guide (dlpu109), we successfully connected to the device through DLP EVM GUI, tested / configured different settings and run it. The connecting and power-on procedures required were always followed. For our application we were trying to work with test patterns, splash images, however due to lack of flexibility (info found on these forums), we ended up using the device in external display mode, projecting some custom patterns on the DMD. Everything was working as expected.

After setting up the device in the lab for the testing, device suddenly cannot be recognized by PC / GUI. We tried with different USB cables, changing jumper from J67 position back to J9 position to start in boot-mode. No matter the jumper position (J67 or J9) LEDs D5, D6, D7 and D15 stays powered ON (D15 does not blink when jumper is on J67). Device is not responsive and can not be detected by PC/GUI. Same cables & power supply was used at first when we were setting the device up, and later in the lab setup - None of the components changed.

Do you have any suggestions how to get back the connection to the device?  
Is there any additional information available, how to identify where the problem is coming from (DLPC7540EVM board or DLO650TE)? 

Thank you very much in advance for any help! 

Best regards, 
Miha