Other Parts Discussed in Thread: DLPDLCR3010EVM-G2, , DLPA2005, DLPA3005, DLPA3000
Hi,
I have several questions about the two evm boards.
Q1: DLPDLCR230NPEVM can be increased to 350 lumens, in this case, DLPDLCR3010EVM-G2 is only 300 lumens out-of-box, then which one is brighter?
Q2: What is the max lumens when replace the dlpa of DLPDLCR230NPEVM from dlpa2005 to dlpa3005?
Q3: DLPDLCR3010EVM-G2 is 300 lumans out-of-box, what could be the max lumens with dlpa3005?
Q4: If I produced 10k evm boards, what are the prices for the two evm boards?
Thanks in advance
All the best,
Jeff XU