This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010: DLP3010

Part Number: DLP3010

Hello everyone,

I have encountered some trouble in long-term using DLP3010 projector according to DLP3010LC-EVM.

When working with trigger in mode by a camera or other controller, at first, the DLP3010 display is normall and Trig2_out signal is correct.

But after a long time, perhaps a few days, the graphics captured by camera become wrong and continue until power cycle the system.

Immediately, I Measured the signals Trig_in and Trig2_out with oscilloscope and the screenshot as below.

The bule line of channel 2 is Trig_in wave form and the yellow line of channel 1 is Trig2_out wave form.

So I think the internal pattern streaming displayed by DLP3010 projector run into incorrect state.

Thanks for any help.

Regards,

Yang