Hi!
I wonder if its possible to adjust the focus distance for these light engines (they seem to be based on a similar design) - especially a changed Throw Ratio would be of interest (so that the projected image gets smaller at a longer distance). That would be of interest because for a planned application a longer distance but still the smallest possible projection size would be required. Since the focusing optics is only screwed onto the light engine: are there alternatives to the standard projection lenses or is there an optical element that can be put infront of the existing projection optic in order to reduce the Throw Ratio?
Thanks in advance,
Dominik