Hi,
I have a Pico Projector development kit that I need to modify for a custom research setup. I'm trying to replace the built-in 3 color LEDs with a single brighter source (controlled externally, not via the kit). When I remove the LEDs and power up the board the red error light comes on (no surprise) and the projector stays on the startup splash screen.
I can't find any info in the manuals re: how the system tests for LEDs on startup. Is it possible to run the board without the LEDs attached? Anything I can do to bypass the internal test to see if LEDs are present? Or any way to add a 'dummy' element that mimics the LED array?
Thanks in advance for any input -
Ian