I am trying to connect the dlp6500 and raspberry pi to use.
Are there any library functions related to the dlp6500?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to connect the dlp6500 and raspberry pi to use.
Are there any library functions related to the dlp6500?
Hello JongHyun,
We do not have Linux libraries for the DLP6500, nor as far as I am aware do we have a Linux USB driver for the DLPC900 board.
You would need to look at the Source code that we provide in the Windows software distribution to see if it can be adapted to Linux. By default after installing the GUI software for the DLPC900 systems it can be found under C:\Texas Instruments-DLP\DLPC900REF-SW-5.0.0\DLPC900REF-SW-5.0.0\DLPC900REF-GUI\Source.
Fizix