All of the documentation describes the pico projector (0.17" pico kit) running at 60 Hz. I presume it will not run faster, but can I run it more slowly?
If I reduce the master clock rate, is there any reason why I cannot run the entire system at 40 Hz? or slower? Is there a lower limit where performance or lifetime is impacted?
thank you,