Other Parts Discussed in Thread: DLP650TEEVM, , DLPC7540, DLP650TE, DLP471TE, DLP471NE, DLP651NE
Dear Team,
I have a set of DLPC7540EVM+DLP650TEEVM evaluation platform in hand now.
When I tried to feed video signals via fpd-link port to DLPC7540EVM, it cannot be recognized correctly and there is no display on DMD.
What I have done:
1. fpd-link connection and electrical characteristics are checked.
2. HDMI to Vx1 input is checked.
3. FPD configration register is checked,
4.I tried to set "Write Source configuration" based on what I got from Step 2, but "0xA excution failed" occurred
So I cannot feed signal via fpd-link port now, and my questions are:
1. how can I find out whether DLPC recognized fpd-link or not?
2. or do I have to set relative configuration rather than waiting for automatically detection?
Thank you
Best regards,
Sherman HUO