Other Parts Discussed in Thread: DLPA2005, DLPC3478, , DLPDLC-GUI, DLPC-API
Application: Customize the display board and main board PCB into a single PCB within certain dimensions (user requirement), to produce an array of 1D patterns at a fixed rate and also trigger cameras.
EVM: DLP3010EVMLC
Major components required on the customised PCB would be Cypress USB to serial converter, MSP430, DLPC3478, DLPA2005 and Flash Memory. (Kindly correct if otherwise)
The following queries are considering that since we are making a customised PCB, a need to establish a connection with the same will be present and individual ICs/microcontroller will need programming.
|
Query No. |
Query |
Source |
|
1. |
What driver will be needed to establish a communication with the customised system? |
DLPU074A – Section 3 |
|
2. |
a. Is the dlpc347x Visual Studio project file to be burned on the 32Mb flash memory (W25Q32JVSSIQ) present on the display board.
b. ‘TI provides software as a firmware image. The customer is required to flash this firmware image onto the SPI flash memory’. By what name is this image available? How to incorporate this file in the customised PCB?
c. ‘A flash component is required to store patterns, the software, and the firmware in order to control the DLPC3478 controller’. What is the significance of this software and by what name is it available? How to incorporate this file in the customised PCB?
|
a. DLP-PICO-DLPC34XX-API — DLP® Pico
b. DLPS111C – Section 7.5 Programming
c. DLPS111C – Section 8.2.1.1 Design Requirements
|
|
3. |
What is the significance of ‘DLP3010EVM-LC_Firmware_v8.0.0_Installer’?
Is it necessary step for the customised PCB? |
DLP3010EVM-LC-FW — DLP 3010 Light Control Firmware >> Order and Start Development
|
|
4. |
What is the significance of ‘DLPx010EVM-LC MSP430 Software Setup’ file? |
DLPX010EVM-LC-MSP430-SW — DLPx010EVM-LC MSP430 HDMI Sample Code >> Order and Start Development
|
|
5. |
Will the Cypress IC, MSP430, DLPC3478 and DLPA2005 also need to be programmed. |
|
|
6. |
a. Are the TRIG_OUT_1 and TRIG_OUT_2 used to control synchronization with 2 cameras respectively. b. What is the significance of these signals in Internal Pattern streaming mode? What is frame trigger and pattern trigger? |
|
|
7. |
In order to generate a particular pattern, is it okay if we make use of DLPDLC GUI’s internal pattern mode and download the firmware which can later be burned on the respective IC? |
|
Requesting you to let me know if I missed any critical element necessary for the customised PCB development.