hello
we are using a dual controller setup of the dlpc900 and would like to read the registers of the slave directly. is that possible?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello
we are using a dual controller setup of the dlpc900 and would like to read the registers of the slave directly. is that possible?
Hello Yoni,
With the way the firmware is currently set up it is not possible to read the registers of the secondary controller directly. We are exploring enabling this for some registers on the secondary controller.
Are there specific items that would be most helpful to be to have access to? Feedback on this will be helpful in determining what registers to make available.
Fizix
Hello Yoni,
Please provide details on which registers you would like to read from both ASICs.
Thank you,
Regards,
Aishwarya
Hi
I will need to read the the following registers from both ASICs:
Hardware Status
System Status
Main Status
Read Error Codes
Thank you
Yoni