Other Parts Discussed in Thread: DLPC900
Hi Team,
A customer want to serialize the LVDS output 4 x 16-bit LVDS data can you suggest what SerDes can be used for it? also what is LVDS data output rate form the DLPLCRC900DEVM?
Regards,
Marvin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
A customer want to serialize the LVDS output 4 x 16-bit LVDS data can you suggest what SerDes can be used for it? also what is LVDS data output rate form the DLPLCRC900DEVM?
Regards,
Marvin
Hello Marvin,
What is the DLPLCRC900DEVM being used for in this case? Can you clarify the end goal? A SerDes is not commonly used with this particular EVM because the DLPC900 does not use an FPGA.
Best,
Maxine
Hi Maxine,
Heres more information:
The plan is to replace 2 X 150-pin cables with a 2 x 50-pin cables. The cables that come with the dev kit are thick and expensive and the customer have been trying to find a way to replace them.
in their design, they have two boards: a DMD formatter board and a DMD board. This setup will require cables. Is there a way to use some other cables if they want to go with the DLPC900 chips?is there an off-the-shelf IC available to Serialize/Deserialize the 4 x 16-bit LVDS interface without using an FPGA.
Marvin,
The dual controller DMD interface has 4 buses (A,B,C,D) each with 18 differential LVDS pairs (16 x D_*, 1 x SCTRL_*, 1 x DCLK_*). DCLK is generally 400MHz. One would need to keep the DCLK to Data & SCTRL timing relationship (setup/hold) with any solution.
In addition, there is an important system timing relationship between the DMD Data interface and the LVCMOS Micromirror Reset Control signals (RESET_ADDR*, RESET_MODE*, RESET_SEL*, and RESET_STROBE) that needs to be maintained. If you add a latency to the DMD Data Interface, you need to add the same latency to the Micromirror Reset Control interface as well.
We are not aware of any off-the-shelf solution to serialize this interface.
A number of customers have used micro-coaxial and/or twin-axial cables (I-PEX, KEL TMC Series, and others). These can often be ordered with the wires bundled, making for a less bulky cable interface.
Regards,
Gary