Hi, I am working with the DLP LightCommander 5500, and am having trouble with the failure of the red LED.
I later found the errata E0031, where it describes that premature failure of red LED(or sometimes the other colour) will occur when the light intensity setting is set to greater than 60%.
Since it has been posted so formally, I figured that many other people have experienced this problem as well.
What kind of solutions are currently available?
Anything will be greatly appreciated.
Yuma