This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC6401: Firmware file

Part Number: DLPC6401
Other Parts Discussed in Thread: DLPC350, TIDA-00782, DLP4500

I'm an engineer for a design house helping a customer update an obsolete DMD + controller.  For the updated design, they've selected the DLP4500 DMD and the DLPC6401 controller.  I have the LightCrafter 4500 and the DLPLCR4500GUI, but it uses the DLPC350.  We're building a board based on the TIDA-00782 reference design which indicates it's been tested.  Where can I get a firmware file for this?

Thanks in advance,

Eric