Why do I set the input source to an extern video port, then set the maximum current and current, and then enable led, and the current value is 0?
executive instruction params
0x05 00 (extern video port)
0x5c rgb value:1023
0x54 rgb value:100
0x52 set red led : 0x01
firmware
my code: