This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DMD blocks time response

Other Parts Discussed in Thread: DLP550HE, DLPC410, DLPC910, DLP650LNIR, DLP9500, DLP7000

I already read with deep interest some questions/answers inside the forum about DMD use. Thanks all

Actually I still have a wonder about the speed response of DMD in Load4 Mode.  I understood that each mirror can switch in 4 us from reset state to ON and than it settles up to ON state in other about 12 us.

When I load with identical data the block, the command will be performed by the mirrors of the block at the same time all togheter? Or each mirror will tilt sequentially from the first up to the last one? 

I.e. if I illuminate the block with a small spot of light I'll see the brightness passing from 100% to 0% in 4-12 us or I'll see a sequence of gray steps of 12us each starting at 100% up to 0% ?

The timing rule of such an operation in case applies also to the blocks of the reset command?

Thanks