Dear TI's friends
I am a sortware engineer coming from Wintech Inc
Hardware = Lightcontrol4710
Operate mode = internal pattern stream
Could you give some advice about how to project only one specified pattern set while there are several pre-stored others in the SPI flash
and each pattern set includes a different number of vertical or horizontal patterns
For example, a vertical pattern set include the maximum 8 pictures, and next horizontal Pattern set consists of 7 pictures
Now, I am going to start projecting the vertical pattern set or horizontal pattern set, rather than both pattern sets to play one by one
I presume that DLPC3479 project all the pre-stored pattern sets according to the specified timings after recieving the "Start Command"
My Operatint Process:
Create a vertical pattern set
Create a horizontal pattern set
Configure Pattern Order Table Entry and program/load pattern set
Send "Run Continuously" command to start projecting
Now , both pattern sets are displaying one by one
Then, I reboot device and change to the advanced operation GUI
First of all, reload pattern sets from the external flash, we can not specify the pattern set so that all the pattern sets will be reload to DLPC3749 internal RAM
Second: send "Start" command, but both pattern set pictures are displayed
So I ask to you share me some information to display specified pattern set only
Thank you for any help
Yours sincerely
Eric