This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCRC900DEVM: Device Not recognize by GUI

Part Number: DLPLCRC900DEVM

Hi There,

I have some problem on DLPLCRC900DEVM while doing testing. Through the JTAG programmer I run successfully programming part. Then after when I try to connect board with DLP Lightcrafter 900 GUI, it thrown an error like device not detect, and the thing is board should be detect if your JTAG program successfully run. In my case program run but device not detect by GUI. I tried by doing replacing master and slave DLP IC's also I was uninstalled GUI and re installed it but still it thrown an error. So could you please suggest me what is the solution of this?

Thanks & Regards

Bharat Navadiya

  • Hello Bharat,

    I'm putting one of our team members in contact with you now. Please note that this site is undergoing maintenance and might not be available. We will make sure to return to your thread as soon as possible.

    Thank you!

    Aaron

  • Hello Bharat,

    It sounds like when you try to connect with USB, the system is not detected.  Even though the JTAG tool appeared to successfully program the boot loader, it is possible that there was some corruption.  I assume this is a new build, so there could be an issue with the Primary Controller Flash.

    I would use the JTAG utility and try the Boot Loader programming process again.  I would run the erase process twice before reprogramming to see if fixes the issue.

    Fizix

  • Please let us know if this resolves your issue?