This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR471TPEVM: Failed to update image, and dlp evm does not work now

Part Number: DLPDLCR471TPEVM
Other Parts Discussed in Thread: DLP471TP,

Hi,

    I downloaded DLP471TP_EVM_v3.2.2_MCU_FW4.5.0.img from ti.com, and connected the DLP EVM GUI 3.1.0.7.exe via USB, then I chose the DLPDLCR471TPEVM as well as usb connection.  After  I clicked  update firmware button , it appeared failure notification. And now the DLP can get into the bootloader mode, but can not read any information if click get button. Please help!

BR,

Jeff Xu

�DLPA����r�|��g}RO%�
��xnT�T�_߮I�܌r���W�wS�ts��R������@_���!<
�Q��ֳ	��U�w׻�s:�%/6l�v�Xǘ>/�q���;�W��#����N�nG9iadH�}����^z�I�:M����j��~�1
�W;���3-���q��R�x��۪h�G$
�Uu�U��Ҹ��X��h������E8C|vs��
�9_��8��:���L{K�<��ؗI8ﭽ���_��7���݃��e��^�
���
3uD�w��B��e�Ψy���v�=���l�lR���+���E�ᵂ�k$���䯀�S2yۢ?���f|&�K�)c0�\�79����(#E��A
i�^N�ݮФo8�]��tZǂ�V,1ݟ)<����e%}.�F�ޤ���^�q��d��q��yY������ƹ��)u�^RR