This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710EVM-LC: DLP4710EVM-LC Trigger out

Part Number: DLP4710EVM-LC

I am utilizing a DLP4710EVM-LC for projecting patterns. To ensure synchronization with a camera, I am employing trigger out 2 for internal patterns. Regrettably, there is a disparity between the output frequency and the designated exposure parameters. I have included an illustrative instance below: when configuring parameters for 30Hz, the oscilloscope records 33.1Hz instead. This discrepancy persists across various frequencies. Could you kindly provide insights into the potential causes of this issue?

Additionally, I am inquiring about the origin of the high-frequency noise apparent atop the trigger signal.
Thank you,